QSPI RAM on OSPI Interface of H7A3 MCU issues
Hi Guys,
I need some help / input:
I am trying to get the communication running between my Nucleo H7A3 and a Shield with a ISSI QuadSPI RAM in a SOP-8 Package running.
Scenario:
I am debugging with my Scope, I have a digital Probe on all 6 lines (CSn, Clock and DIO0-3) and I can see the communication.
First issue:
I am sending the command "0x05 - read mode register". I can see the outgoing communication on the scope, I can see the incoming communication on the scope. I can see on the scope that the RAM is sending a response - with the default Mode Register Value. But the Variable I am reading ins, is not updated with that value.
My Code:
OSPI_RegularCmdTypeDef cmd = {0};
uint8_t buf[4] = {0,};
cmd.Instruction = SRAM_CMD_RDMR; // instruction byte
cmd.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE; // mode of the instruction
cmd.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS; // size of the instruction
cmd.DataMode = HAL_OSPI_DATA_1_LINE; // data mode: 1 Line
cmd.NbData = 1; // number of data transfered with the command
cmd.DummyCycles = 0x00; // number of dummy cycles before data phase
HAL_StatusTypeDef status;
status = HAL_OSPI_Command(hSramOSPI, &cmd, HAL_OSPI_TIMEOUT_DEFAULT_VALUE);
if(HAL_OK != status) {
return(1);
}
status = HAL_OSPI_Receive(hSramOSPI, buf, HAL_OSPI_TIMEOUT_DEFAULT_VALUE);
if (HAL_OK != status) {
return(1);
} else {
SRAM_modereg = buf[0];
}
I see literally in the scope 2 Bytes: 0x05 (=read Mode register command) and the response 0x40 - which is the default value of the chip according to its datasheet. But the buf variable, as well as the SRAM_modereg variable, where it is copied to remain 0.
I am using the MCU, the D-Cache and the I-Cache - Am I running in some weird Cache issues here - even if I am using OSPI in Blocking mode? Are there some DMA Transfers in the Background I am not aware of or something similar?
Second Issue:
If I use anything other than
cmd.AddressMode = HAL_OSPI_ADDRESS_NONE;
like 1 Line or 4 Lines for the address Phase, there is no communication at all on the bus. If I disable the Address phase, I can see communication on the both no matter which mode (SPI or QSPI) I am in. My Code:
static uint8_t rOS_SRAM_read(uint32_t addr, uint8_t * pData, uint32_t dataSz) {
// @brief read from SRAM in Quad-Mode (Blocking)
// @PAram u32 addr: address
// @oaram u8* data: read buffer pointer
// @PAram u32 dataSz: # of data to be read
// @return u8 status: 0 = OK (no error)
if (pData && dataSz) {
OSPI_RegularCmdTypeDef cmd = {0};
cmd.Instruction = SRAM_CMD_READ; // instruction byte
cmd.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS; // size of the instruction
cmd.Address = addr; // data address
cmd.AddressSize = HAL_OSPI_ADDRESS_24_BITS; // size of the address (typ. 24 bit)
cmd.NbData = dataSz; // number of data transfered with the command
if(SRAM_quad) {
cmd.InstructionMode = HAL_OSPI_INSTRUCTION_4_LINES; // mode of the instruction
#ifndef SRAM_NOADDR
cmd.AddressMode = HAL_OSPI_ADDRESS_4_LINES; // send an address?
#endif
cmd.DataMode = HAL_OSPI_DATA_4_LINES; // data mode: send data or just command
cmd.DummyCycles = 0x2; // number of dummy cycles before data phase
} else {
cmd.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE; // mode of the instruction
#ifndef SRAM_NOADDR
cmd.AddressMode = HAL_OSPI_ADDRESS_1_LINE; // send an address?
#endif
cmd.DataMode = HAL_OSPI_DATA_1_LINE; // data mode: send data or just command
}
HAL_StatusTypeDef status;
status = HAL_OSPI_Command(hSramOSPI, &cmd, HAL_OSPI_TIMEOUT_DEFAULT_VALUE);
if(HAL_OK != status) {
return(1);
}
status = HAL_OSPI_Receive(hSramOSPI, pData, HAL_OSPI_TIMEOUT_DEFAULT_VALUE);
if (HAL_OK != status) {
return(1);
}
}
return(0);
}
No communication at all means: No Chip Select, No Clock, all data lines are idle in the Scope. The OSPI peripheral simply does nothing.
I have some experience with QSPI SRAM on an G4, but I am new to the OSPI Peripheral on the H7. Is there any major differences in the behavior of the QSPI functionality I am not aware of and therefore stumbling over? My approach was similar to that what I got successfully running on an G4, but I have absolutely no Idea why the H7 OSPI-Peripheral would simply do nothing at all, when I add an address phase!?
Any Help / input is appreciated! Thanks guys!