Skip to main content
Explorer
June 10, 2025
Question

Question about STM32H7 SDMMC2 and UHS-I mode support

  • June 10, 2025
  • 1 reply
  • 454 views

Hello,

When I read though AN5200 (Getting started with STM32H7 Series SDMMC host controller), I am not sure I fully understand the statement about UHS-I mode support in Table 2. (SDMMC1 and SDMMC2 main features) as in below screenshot, 

Screenshot 2025-06-10 at 12.15.49 AM.pngScreenshot 2025-06-10 at 12.15.57 AM.png

The table states that SDMMC2 does not have control signals for external voltage switch transceiver, but it also states in footnote that it seems can support a transceiver with bus direction sensing without the need for direction control signals.

I can not find further information in documents about how UHS-I mode on SDMMC2 is implemented, but what in the above table and the footnote implies it is possible. so I would like to ask here to confirm that

1) if UHS-I mode support can be achieved on SDMMC2 port, without direction control signals, and 

2) As no clock feedback input pin and direction control pin on SDMMC2 port, are these pin actually not needed in this scenario? Thus a level shifter with bus direction sensing like TXB0108 (from TI) will be all that needed to do the job, 

Thank you.

/Roland

 

 

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    July 2, 2025

    Hi @Rolandash ,

    SDMMC2 supports only Default and high-speed (no UHS mode).

    However, the UHS-I mode support can be achieved on SDMMC2 without direction control signals ONLY in case you use a bus direction sensing level shifter. 
    Clock feedback input and direction control pins are not needed in this scenario. The level shifter with bus direction sensing will handle the necessary signal direction and voltage switching.

    -Amel

    RolandashAuthor
    Explorer
    July 2, 2025
    Thank you @Amel for confirming my question.

    Is there a reference implementation circuit of UHS-I on SDMMC2? Like what is the recommended part of level shifting and voltage switching with direction sensing?

    I could not find these information in the documents, and the internet as well.

    Technical Moderator
    July 3, 2025

    Hi @Rolandash ,

    Unfortunately, I don't have a reference that I can recommend.

    -Amel