RAMECC with Dcache
I am working on a Nucleo-H753ZI board looking at RAMECC.
My code is based on the example at
https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/NUCLEO-H745ZI-Q/Examples/RAMECC/RAMECC_ErrorCount
I am using debug to watch the status of the RAMECC registers at HAL_RAMECC_IRQHandler in stm32h7xx_hal_ramecc.c using Memory Browser.
I get sensible numbers, such as:
0x52009024 RAMECC_M1SR 00000001
0x52009028 RAMECC_M1FAR 00000174
0x5200902C RAMECC_M1FDRL BB6A6546
0x52009030 RAMECC_M1FDRH 0488EBAA
0x52009034 RAMECC_M1FECR 00000031
However, if I turn on Dcache using SCB_EnableDCache(); in main.c I mostly get 0x03 in RAMECC_M1SR,
which would suggest both a single and double error.
Does it make sense to have a status of both single and double error if Dcache is turned on?
If yes what sort of error do I treat it as in terms of correcting it (do I assume it is a double error and therefore not correctable)?
If not is there something I can do so that only 0x01 or 0x02 appears in RAMECC_M1SR with Dcache enabled?