Read While Write in STM32U5A9J-DK
Hi Team,
We are working on STM32U5A9J-DK for one of our application interfaced with Octal SPI Flash.We needed to acheive RWW operation which is supported by our Flash chip and we have used OSPI1 and OSPI2 in multiplexed mode but we are controlling Chip select in software because of the limitation in STM32U5A9 chip and we were able to see Parallel operation of Write and Read which is RWW but an issue is we are unable to read the Bank stat register from the flash chip which gives information of the Bank number which is being Written while Read is happening. Now our doubt is it because of chip select controlled in software its not able to read volatile register properly?
Any input on this?
Sanath