Skip to main content
Explorer II
September 18, 2024
Question

Request for HM01B0 Camera Module Drivers for STM32

  • September 18, 2024
  • 0 replies
  • 613 views

Hello,

Hello,

I am seeking either a ready-to-use or partially implemented driver for the  HM01B0 - QVGA SPI Camera Module to use with the NUCLEO-F767ZI board.

My aim is to recreate a project I previously completed with the Portenta H7 on the OpenMV IDE, but this time I want to write the code in C instead of MicroPython.

The goal is to optimize the project, gain a deeper understanding of the hardware, and move further into embedded systems development with something I'm already familiar with.

Any advice or suggestions are also greatly appreciated!

Thank you in advance,
Moustafa

 

    This topic has been closed for replies.