Resistor configurarion used for VBUS configuracion
Hi, I´m reading the following document : "an4879-introduction-to-usb-hardware-and-pcb-guidelines-using-stm32-mcus-stmicroelectronics" to implement USB in my application.
In section 2.6.1 Simple Resistor Divider it says "This solution works well as long as GPIO maximum operating conditions are >= VDD+ 3.6 V" this must be meet to use the following voltage dividider

I´m going to use PA9 pin, in the datasheet of my MCU STM32L4P5RGT6 it states this pin is 5V tolerant
As I understood this pin doesnt meet the condiciton mentioned before because my VDD=3.3V and so GPIO maximum operating condition should be >= VDD+3.6V so we have 3.3+3.6V=6.9V so 5V < 6.9V so I can't use this configuration do I understand this well ?
Should I use this other configuration?

I´m a bit confused about it hope some one could help me to clarify this.