Skip to main content
Visitor II
December 11, 2024
Solved

RK043FN8H-CT672B for STM32F756BGT6?

  • December 11, 2024
  • 2 replies
  • 1225 views

Do I need to use RK043FN8H-CT672B for STM32F756BGT6?

    This topic has been closed for replies.
    Best answer by mƎALLEm

    Hello @Mimikakarlo and welcome to the community,

    According to the datasheet yes and you need to drive it with LTDC interface over RGB lines.

    For more details please refer to the AN4861 "Introduction to LCD TFT display controller LTDC on STM32 MCUs"

    Hope it helps.

     

    2 replies

    Super User
    December 11, 2024
    Visitor II
    December 11, 2024

    yes

    mƎALLEmAnswer
    Technical Moderator
    December 11, 2024

    Hello @Mimikakarlo and welcome to the community,

    According to the datasheet yes and you need to drive it with LTDC interface over RGB lines.

    For more details please refer to the AN4861 "Introduction to LCD TFT display controller LTDC on STM32 MCUs"

    Hope it helps.

     

    Visitor II
    December 11, 2024

    Thank you for youe answer. I have a problem with the RK043FN66HS-CTG display because i want brightness 1000cm/m^2, can you suggest me another display for STM32F756BGT6 with 4.3in, 480 x 272 pixels and 1000cm/m^2?
    Thank you!

    Technical Moderator
    December 11, 2024

    This is what is used on STM32H743-Eval board: AM-640480G5TNQW-T00H