RM0360 and stm32f030xc.h TIM7 IRQ discrepancy
I am designing a board based around the STM32F030RC, and noticed an apparent discrepancy on IRQ18 between materials.
STM32CubeMX allows both TIM6 and TIM7 to generate interrupts, and the stm32f030xc.h file it generates defines TIM6 as IRQ17 and TIM7 as IRQ18. However, the RM0360 Reference Manual claims that IRQ18 is Reserved, and does not list an interrupt for TIM7, only for TIM6.
My question is: is IRQ18 generated by TIM7 like STM32CubeMX claims or is it Reserved like RM0360 claims?
/*!< Interrupt Number Definition */
typedef enum
{
/****** Cortex-M0 Processor Exceptions Numbers **************************************************************/
...
/****** STM32F0 specific Interrupt Numbers ******************************************************************/
...
TIM1_BRK_UP_TRG_COM_IRQn = 13, /*!< TIM1 Break, Update, Trigger and Commutation Interrupt */
TIM1_CC_IRQn = 14, /*!< TIM1 Capture Compare Interrupt */
TIM3_IRQn = 16, /*!< TIM3 global Interrupt */
TIM6_IRQn = 17, /*!< TIM6 global Interrupt */
TIM7_IRQn = 18, /*!< TIM7 global Interrupt */
TIM14_IRQn = 19, /*!< TIM14 global Interrupt */
TIM15_IRQn = 20, /*!< TIM15 global Interrupt */
TIM16_IRQn = 21, /*!< TIM16 global Interrupt */
TIM17_IRQn = 22, /*!< TIM17 global Interrupt */
...
} IRQn_Type;
STM32CubeMX
Table 31. Vector table