Skip to main content
Visitor II
October 19, 2025
Solved

RM0390 typo

  • October 19, 2025
  • 2 replies
  • 496 views

Documentation: RM0390
Revision: Rev 7, June 2025

Section 26.3.2 Page number 830:

Under Simplex communications, it says the RXONLY bit is in the SPI_CR2 register but the register map confirms RXONLY bit is in the SPI_CR1 register.

    This topic has been closed for replies.
    Best answer by Issamos

    Hello @zebra_scopper76 

    This is a minor typo on the Simplex communication paragraph. I think @Imen.D you may help reporting this issue to be rectified on the future.

    Best Regards.

    II

    2 replies

    IssamosAnswer
    Graduate II
    October 19, 2025

    Hello @zebra_scopper76 

    This is a minor typo on the Simplex communication paragraph. I think @Imen.D you may help reporting this issue to be rectified on the future.

    Best Regards.

    II

    Technical Moderator
    October 20, 2025

    Hello @zebra_scopper76 , @Issamos 

    Thank you for having reported this.

    An internal ticket number 219990 is submitted to fix this typo in the coming release of RM0390.
    (PS: Ticket number 219990 is an internal tracking number and is only for reference. It is not accessible or usable by customers).