RM0394 SRAM2 connectivity in bus matrix
In the lower-end STM32L4, covered by RM0394, SRAM is partitioned into two parts, SRAM1 and SRAM2.
SRAM2 (besides being "special" in that it has ECC and automatic erase facities), is mapped at both 0x1000'0000 and at the end of SRAM1 in the 0x200x'xxxx area.
In Figure 1 System architecture, SRAM2 does not have the connection needed for that second mapping, i.e. to the S-bus of the processor.

JW