Skip to main content
Explorer
May 5, 2025
Question

RTC Calibration

  • May 5, 2025
  • 2 replies
  • 467 views

I have selected the RTC calibration as 512Hz. Will I be able to perform RTC smooth calibration if my frequency obtained on the RTC calib pin is beyond the range 511.75Hz - 512.25Hz. 

How do I calibrate the RTC beyond this range ?? 

 

    This topic has been closed for replies.

    2 replies

    Super User
    May 5, 2025

    From the reference manual:

    The RTC frequency can be digitally calibrated with a resolution of about 0.954 ppm with a
    range from -487.1 ppm to +488.5 ppm.

    If your crystal is outside of those limits, you will be unable to calibrate it with this method. Since crystals are typically accurate to well under 100 ppm, there is plenty of margin.

     

    If your clock is outside of that range, choosing a more accurate clock source is probably the best option.

    J_ThomasAuthor
    Explorer
    May 7, 2025

    Thank you so much!

    Graduate
    May 6, 2025

    Double check which oscillator you are using for RTC - some time it uses as default internal RC instead of external crystal.