RTC_OUT availability while STM32H7 is powered off
Hi,
I'm using an STM32H7 microcontroller and need to get the RTC working.
I set RTC_OUT to 1Hz and set the LSE to a 32.768Hz crystal, and inserted the CR2032 battery.
When the microcontroller is powered (VDD 3V3), I see the waveform oscillating at a frequency of 1Hz.
My question is: should the signal on the RTC_OUT pin remain when I remove the power?
Thanks