Running STM32U083 directly from Li-SOCL2 battery
I am using STM32U083 MCU in a project that runs on a 3.6v Li-SOCL2 lithium thionyl chloride battery (OC voltage 3.65V / Nominal voltage at 1mA 3.6V).
Currently I have used a LDO of 2.5v to power the MCU, but I was thinking if we can eliminate the LDO and directly power the MCU from the battery.
Going through the datasheet I have found that the recommended input supply voltage is 1.55v-3.6v, and max is 4.0v, I have seen a mass produced device using the same battery directly on a STM32L053 MCU. I am expecting the same might be possible with U083 as well.
Please suggest if this is okay or is there can be any potential issues that can happen.