RXP bit not being after SPI transfer
Hello all,
I have been struggling with DMA transfers from SPI transactions and would love a second opinion on what I could be doing wrong. I have confirmed that polling works and I can corroborate the data I see in the RX registers with a scope.
I do not use the HAL API for SPI receptions with DMA, I am mostly using low-level register modifications to trigger read/writes from the SPI peripheral, although I do use the initialization of the peripheral that is generated by Cube IDE.
I was looking into why the DMA destination buffer was not being filled, when I realized there was something wrong with the SPI transaction itself. According to the RM, the DMA will make a request once RXP is set and it is automatically activated according to `RXWNE` and `RXPLVL`. When inspecting these register during the transaction I see that `RXWNE` is set to 1, meaning there is, at least, 4 bytes in the RX FIFO. RXPLVL itself reads all zeroes since the data size is larger than 16 bits, so I don't see an issue there.
The transaction is completed correctly, as the EOT flag is raised and I see the data in the RXDR registry (and is cleared out once the EOT flag is set).
The transaction is a 32 bit from an AD with an 20MHz SPI clock that occurs after a GPIO interrupt and a timer trigger. These are the settings for my SPI peripheral:
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_32BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_ENABLE;
hspi1.Init.CRCPolynomial = 0x0;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
hspi1.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi1.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi1.Init.MasterSthat RXWNE SIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;
hspi1.Init.ReadyMasterManagement = SPI_RDY_MASTER_MANAGEMENT_INTERNALLY;
hspi1.Init.ReadyPolarity = SPI_RDY_POLARITY_HIGH;This is the simplified code I use for the transaction:
HAL_GPIO_WritePin(css_gpio.GPIO_PORT, css_gpio.GPIO_PIN, GPIO_PIN_RESET);
SCB_InvalidateDCache_by_Addr(&spi_buffer_rx[buf_index], sizeof(uint32_t));
// set up dma BEFORE doing the transfer
HAL_DMA_Start(hspi1.hdmarx, (uint32_t)&hspi1.Instance->RXDR, (uint32_t)&spi_buffer_rx[buf_index], 1);
hspi1.Instance->CR1 &= ~SPI_CR1_SPE; // disable the SPI per before amking changes
hspi1.Instance->IER |= SPI_IER_RXPIE; // enable the interrupts from RXP
// enable the DMA before starting the transfer
hspi1.Instance->CFG1 |= SPI_CFG1_RXDMAEN;
hspi1.Instance->CR1 |= SPI_CR1_SPE;
hspi1.Instance->TXDR = 0UL; // send an empty array
hspi1.Instance->CR1 |= SPI_CR1_CSTART; // start the transfer and wait until it's done
//while(!(hspi1.Instance->SR & SPI_SR_RXP)); // wait for the hardware to set the flag of an available packet in the FIFO. This SHOULD trigger the DMA transfer
uint32_t my_val=hspi1.Instance->RXDR;
while(!(hspi1.Instance->SR & SPI_SR_EOT));
hspi1.Instance->IFCR |= SPI_IFCR_EOTC | SPI_IFCR_TXTFC; // clear the flags for end of transfer and txt sr
HAL_GPIO_WritePin(css_gpio.GPIO_PORT, css_gpio.GPIO_PIN, GPIO_PIN_SET);Does anyone have an idea why RXP is not being set even though I have a successful data reception? I suspect it has to do with data packing, but I've set the peripheral to the best of my knowledge.
Thanks!