Skip to main content
Graduate
October 9, 2024
Solved

SDIO port with 2 SDCARD Chip Select

  • October 9, 2024
  • 1 reply
  • 1058 views

Hello, 

I have a STM32F411 and I am ready using the SDIO port, 

I would like to connect 2 SDCARD to the SDIO port and be able to switch from one to another like using a CS Chip select GPIO. 

Is it possible ? how would I do that ? 

Thanks 

Vincent 

 

    This topic has been closed for replies.
    Best answer by STTwo-32

    Bonjour @vbesson 

    As you can see on the paragraph 3.26 of the DS10314, you can only use only one SD Card each time.

    Best Regards.

    STTwo-32 

     

    1 reply

    STTwo-32Answer
    Technical Moderator
    October 9, 2024

    Bonjour @vbesson 

    As you can see on the paragraph 3.26 of the DS10314, you can only use only one SD Card each time.

    Best Regards.

    STTwo-32