SDMMC peripheral in STM32L4A6 unable to run with the uSD card using 1.8V IO
I have a new board design that interfaces an STM32L4A6 with a uSD card using 1.8V I/O. The SD Card is powered by 3.3V and supports the LVS mode of SD. The STM32L4 does not seem take account the SD specification 6.0. There is no auto detection mecanism of the signalling voltage level in this MCU. This MCU can not start in UHS-I 1.8V mode.
Do you know a MCU which can start the LVS identification sequence ?