Question
Seeking Recommendations for Dual-Core STM32 Microcontrollers
Hello everyone,
I am currently working on a project that requires a dual-core microcontroller with the following specifications:
- Flash Memory: 256 KB to 1 MB
- RAM: 16 KB to 64 KB
- Architecture: 16-bit / 32-bit MCUs
- RTOS Support: Yes
- Clock Frequency: 48 MHz to 100 MHz
- Core: Dual core
- Over The Air programming: Yes
I would greatly appreciate your suggestions on the best STM32 models that meet these criteria. If you have experience with any specific models, please share your insights regarding their performance, ease of use, and any potential drawbacks.