Selection of STM Eval Board
Hi
I' am devloping an Hardware using STM32G491RET6 where I'm using many interfaces such as I2C, SPI, RTC, USB, RS232, ETH etc.
The above hardwase is not yet fabricated, but we want to develp a software before the fabricated board arrive. Hence in order to develop the code which Eval Board is required.
The one which is availabel "NUCLEO-G491RE", this has only IO access available but does not have any trascivers onborad where we cannot interface.
Kindly suggest the Eval board where I can use maximum interfaces as mentioned.
Regards