Seting up ADC in dual mode with DMA - Manual is not satisfying.
I have some problems getting all the information out of the manual.
Using HAL is no option.
There are a lot of questions (Question are all refering to "Injected simultaneous mode") that cant be answered, or details that are confusing:
- When in Injected simultaneous mode, regular conversions are possible, but use the settings of the common registers for dual settings?
- Picture "say what": It does not really say how it would behave in that case.
- With all the information i gathered, i can not really determine, how the ADC would work in combination with DMA. When i start regular conversions on ADC2, is it then considered dual mode?
It would be helpful to have a checklist, or a table, that show what has to be orcan be set in different modes. Is there such information availlable? Or anyone knows of a good tutorial?