Setting FDCAN port parameters of STM32G0B1x for communication with CAN2.0 device
Hi,
I am using STM32G0B1x MCU on my custom hardware and using built in FD CAN controller for communication with external CAN 2.0 device. ATA6560/1 is the CAN transceiver chip from Microchip I am using on my custom board. As per datasheet this chip is CAN FD ready.
I have gone through application note AN5348 and also video - https://www.youtube.com/watch?v=xGRvVKfs2-0 for using FDCAN in normal operating mode. It tells me to use kvaser tool to calculate values for parameters for CAN controller settings. I used this tool with following inputs to achieve Nominal and Data bit rate as 125Kbps.

My external CAN2.0 device works at 125Kbps.
I got calculated parameter values as below:

I was able to set values for Nominal parameters but for Data parameters, calculated values are far away out of range and STM32CubeIDE is a not allowing me to set these values. As per calculation, Data SJW = 255 but tool says its value can be between 1 to 16.

Same is issue with Data Time Seg1 and Data Time Seg 2. Calculated values are 256 and 255 respectively while max value as per tool should be 32 and 16 respectively.
Please help with this issue.
Thanks,
Pradeep