Setting IFCR does not clear ISR
I'm using the STM32F103C8T6, and trying to blink my LED via the interrupt handler of a DMA with this code
#include <stdint.h>
// STM32F103C8 is a medium density device, hence we use the xB header
#include <stm32f103xb.h>
#if !defined(__SOFT_FP__) && defined(__ARM_FP)
#warning \
"FPU is not initialized, but the project is compiling for an FPU. Please initialize the FPU before use."
#endif
int main(void) {
uint32_t blinking[2] = { GPIO_BSRR_BR8, GPIO_BSRR_BS8 };
uint32_t dest = 0;
RCC->CR |= RCC_CR_HSION;
while ((RCC->CR & RCC_CR_HSIRDY) == 0)
;
RCC->AHBENR |= RCC_AHBENR_DMA1EN; // Enable clock for DMA1
RCC->APB2ENR |= RCC_APB2ENR_TIM1EN; // Enable clock for TIM1
RCC->APB2ENR |= RCC_APB2ENR_IOPAEN; // Enable IO port A
NVIC_EnableIRQ(DMA1_Channel2_IRQn);
DMA1_Channel2->CCR |= DMA_CCR_MSIZE_1 // 32-bits memory size
| DMA_CCR_PSIZE_1 // 32-bits peripheral size
| DMA_CCR_MINC // Memory increment
| DMA_CCR_CIRC // Circular mode
| DMA_CCR_DIR // Read from memory
| DMA_CCR_HTIE // Enable half transfer interrupt
| DMA_CCR_TCIE // Enable complete interrupt
| DMA_CCR_MEM2MEM
;
DMA1_Channel2->CNDTR = 2;
// DMA1_Channel2->CPAR = (uint32_t)&GPIOA->BSRR;
DMA1_Channel2->CPAR = (uint32_t) &dest;
DMA1_Channel2->CMAR = (uint32_t) blinking;
TIM1->CCMR1 |= TIM_CCMR1_OC1M_0;
TIM1->DIER |= TIM_DIER_CC1DE;
TIM1->CCER |= TIM_CCER_CC1E; // Enable OC1 output
TIM1->BDTR |= TIM_BDTR_MOE;
TIM1->PSC = 512 - 1;
TIM1->ARR = (15625 * 2) - 1;
GPIOA->CRH &= ~(GPIO_CRH_CNF8 | GPIO_CRH_MODE8); // GPIO A: Clear pin 8 configuanaration
GPIOA->CRH |=
GPIO_CRH_MODE8; // GPIO A: Set pin 8 to output with 50 MHz and push-pull
DMA1_Channel2->CCR |= DMA_CCR_EN;
TIM1->CR1 |= TIM_CR1_CEN;
/* Loop forever */
for (;;) {
}
}
void DMA1_Channel2_IRQHandler() {
if ((DMA1->ISR & DMA_ISR_HTIF2) != 0) {
GPIOA->BSRR = GPIO_BSRR_BR8;
}
if ((DMA1->ISR & DMA_ISR_TCIF2) != 0) {
GPIOA->BSRR = GPIO_BSRR_BS8;
}
DMA1->IFCR = DMA_IFCR_CGIF2 | DMA_IFCR_CHTIF2 | DMA_IFCR_CTCIF2;
}However, at 67, setting the IFCR register does not seem to clear the ISR flags and the handler keeps getting called. How do I handle this?