Shorting of Pin4/Pin8, Pin20/Pin30,Pin49/Pin52,Pin58/Pin59 in STM32G431MBT6 for HART OUTPUT Feedback
Hi Team,
We are currently using ST Micro controller STM32G431MBT6 on our project.
We are shorting the following pin combinations for HART output feedback which serves as an input to the HART Out generator:
PC15(Pin4) and PC0 (Pin8);
PA6 (Pin20) and PE7(Pin30);
PD10(Pin49) and PC6(Pin52);
PA10(Pin58) and PA11(Pin59)
Kindly confirm that this will not create any impact on the normal operation of the controller.
Hoping for your esteemed quick reply.
Best Regards,
Sreejith