Solved
Simple questions about ADC input pin when doing ADC calibration
Hello ST Experts,
I'm using STM32H747 and I try to run adc calibration at the start of the code, like under lines.
HAL_ADCEx_Calibration_Start(&hadc3, ADC_CALIB_OFFSET_LINEARITY, ADC_SINGLE_ENDED);
HAL_ADCEx_Calibration_Start(&hadc3, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED);
I'm wondering if there is a need to apply a specific voltage to the ADC input lines before calling the above functions.