Sine wave generation using DAC
Hello everyone,
I am trying to generate sine wave using DAC and interrupts in my STM32F446 board. I want to do it without using array model. I am getting b infinite_loop when the program is run in debug mode. I have initialised "use float with printf/scanf" settings. The code is as follows:-
#include "stm32f4xx.h"
#include <math.h>
volatile float data;
#include "dac_sine.h"
#define pi 3.14159265359
volatile uint32_t theta = 0;
volatile uint32_t del_theta = 1;
float value;
void dac_sine_gpio_init(void)
{
RCC->AHB1ENR |= (1U<<0); //enable clock for GPIO Port A
GPIOA->MODER |= (0b11<<10); //setting PA5 in analog mode
GPIOA->MODER |= (0b11<<8); //setting PA4 in analog mode
}
void dac_sine_timer_init(void)
{
RCC->APB1ENR |= (1U<<29); //Clock access to DAC Enabled
RCC->APB1ENR |= (1U<<0); //clock access to Timer2 Enabled
TIM2->PSC = 1; //setting pre-scalar value
TIM2->ARR = 999; //setting ARR value
TIM2->CR1 = (1U<<0); //counter enabled
TIM2->DIER |= (1U<<0); //update interrupt enable
DAC->CR |= (1U<<0); //DAC Channel 1 is enable
NVIC_EnableIRQ(TIM2_IRQn);
}
void tim_callback(void)
{
theta = theta + del_theta;
if (theta > 999) {theta = 0;}
float sine_value = sin((theta*2*pi)/1000);
uint32_t dac_value = (uint32_t)((sine_value + 1)*999);
//if (theta > (2*pi)) {theta = 0;}
//data = sin (theta); //statement for sine waveform
//uint16_t dac_value = (uint16_t)((data+1)*0.5*4095);
DAC->DHR12R1 = theta; //statement to load the data in channel 1 of DAC
}
void TIM2_IRQHandler(void)
{
if (TIM2->SR & (1U<<0)) //check if update interrupt flag is raised
{TIM2->SR &=~ (1U<<0);} //clear the flag
tim_callback(); //go to this callback function
}
can someone pls help me getting sine values in live expression windows please.
thanks in advance.