SMPS fail to supply Vcore, what could be happen?
Hi,
I'm using a STM32H757XIH6 with SMPS. Everything (firmware & hardware) are working fine but after a switch off/on of the power supply, I could not connect to the microcontroler via SWD.
First I thought it was the Power configuration that had been corrupted. So I tried to connect in bootloader mode (BOOT0 pin at VDD) , but it doesn't work. I couldn't not connect. You could find in attachment the power supply schematic.
After some investigations, I feel that the SMPS was broken (400mV on Vcap) and the Vcore wasn't supply anymore. So I replaced the SMPS by an external LDO (1.2V). I succeed to connect to the microcontroler.
What I undertsand from the reference manual (chapter 7.4.1 - page 276) is that the microcontroler will stay in reset mode while the Vcore is not correct. I assume we stay in this state because Vcore was about 400mV. It's why, we could not connect anymore to the microcontroler.
=> the SMSP seems broken.
Do you already encountered such problem?
Do you have some suggestions to find the root cause of this failure (ESD, high voltage, high current, others, ...)? Which extra tests can be done to find the root cause?
According to you, is it an irreversible failure or can we recovery the SMPS?
How is it possible to break the SMPS?
Thanks in advances for your help