SMT32F042K6T7 temperature issue
Hello,
I am using STM32F042K6T7 microcontroller for doing some start-up configuration for some Ethernet PHYs by SMI, it is working well at room temperature, and cold (-40°C), but when I increase temperature max (+74°C) the microcontroller it seems is not able to start-up because the SMI signals (MDIO and MDC) seems not to work, I did some test with a Nucleo-F042K6 which has the STM32F042K6T6 heating up the microcontroller up to +74°C and it seems not having the same issue then I would like to make sure that my understanding is correct.
It suppose STM32F042K6T6 has a operating temperature of -40°C to 85°C and
STM32F042K6T7 has an operating temperature of -40°C to 105°C, then in my understanding this is more robust to high temperature, do you have any idea of what could be happening?