Skip to main content
Visitor II
January 2, 2024
Question

SMT32F407VGT6 / CAN issue

  • January 2, 2024
  • 2 replies
  • 1419 views

主控板 (SMT32F407VGT6)与同服板 (STM32F407VGT6) 之间的CAN通讯,环境温度低于-10度,通讯不正常,环境温度高过-10度!

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    January 2, 2024

    Hello @JACK00 ,

    In next time, could you please describe your issue in English as other community members can help you?

    Translation:

    "The CAN communication between the main control board (SMT32F407VGT6) and the server board (STM32F407VGT6), the ambient temperature is lower than -10 degrees, the communication is abnormal, and the ambient temperature is higher than -10 degrees!"

    Not sure the question is clear. Could you please elaborate more?

    JACK00Author
    Visitor II
    January 2, 2024

    The CAN communication between the main control board (SMT32F407VGT6) and the same server board (STM32F407VGT6) shows that the ambient temperature is below -10 degrees, the communication is abnormal, and the ambient temperature is above -10 degrees! Immediately returning to normal, may I ask what the reason is? Confirm that the CAN communication interface hardware chip meets the requirements!

    Technical Moderator
    January 29, 2024

    What is your clock source? HSI or HSE?

    Graduate II
    January 2, 2024