Skip to main content
Visitor II
January 2, 2024
Question

SMT32F407VGT6 / CAN issue

  • January 2, 2024
  • 1 reply
  • 788 views

The CAN communication between the main control board (SMT32F407VGT6) and the same server board (STM32F407VGT6) shows that the ambient temperature is below -10 degrees, the communication is abnormal, and the ambient temperature is above -10 degrees! Immediately returning to normal, may I ask what the reason is? Confirm that the CAN communication interface hardware chip meets the requirements!

    This topic has been closed for replies.

    1 reply

    Graduate II
    January 2, 2024

    Check performance of external clock and transceiver. 

    You can output HSE via PA8 (MCO) and check clock accuracy within specification limits.