SPI 8-Bit frame
Hi,
I hope this is the right place to ask. I'm currently working on interfacing an SD Card with a nucleo f767. I used the DS-Bits in CR2 to set the data frame to 8 Bit (what also should be the reset value). Despite that, MOSI always sends the whole data register, which is 16 Bits. So if I use the function below to send 0xFF, the hardware will send 0x00FF. Does anybody know this issue?