SPI communication with AD9959 4 channel MSPS DDS analog device
Hi, I'am currently working on implementing a driver with the AD9959 with the stm32G474re discovery board, I am able to write to all 4 channel to generate any frequencies with any phases with the SPI module, but when I'm trying to read, HAL_SPI_Receive() gives back a receive buffer with zeros values, I don't understand why, is there anyone who is working on some analog device product and encoutered a similar problem, I'm using spi3 on full-duplex master mode, I probe my sck, MISO and MOSI signal, I can see that the MOSI signal have a correct behaviour, but the MISO signal nevet gets updated even though I programed the device to go on single bit 3 wire mode. Insted, the MOSI signal is changing. At first, I though that my write function was wrong, but it doesnt seems to be the case since I can disable the selected channel, and program any frequencies for each channel by having programmed the 3 wire mode, if it's not on 3 wire mode the code don't work anymore. Here is my write and read function. In the read function, the AD9959_SPI_Transfer() function is calling HAL_SPI_Transmit() to send the read byte instruction. In the read function, the received buffer, receidata is always 0.
Any help would be gladly appreciated!