SPI FULL Duplex Slave ; receive data, but not transmission
Dear Forum
Im using the SPI of STM32 H7 43ZI.
-In master mode,full duplex, not problem: Transmit and receive data precisely, up to 2Mbit/sec (limits come from cable lenght) .Each pack is 24 bytes.
-In slave mode, this is what i do (master at 200Kbit/sec):
a)FIFO LEVEL=2 BYTES
b)Master send 2 bytes . The STM32 Slave Receive this 2 byte , and INT roudine is activate
c) save in a buffer , and load 2 byte to be TX.
And repeat, up to 24 bytes.
Problem is:
* I get 24bytes ok
*no data are trasmitted.. MISO is fix to low
The simplified version of code is this:
//SPI3 Slave
uint8_t *p_TXDR_SPI3= &(SPI3->TXDR);
uint8_t *p_RXDR_SPI3= &(SPI3->RXDR);
void INT_SPI_3_RXTX_8BIT(SPI_HandleTypeDef *hspi3)
{
if ( ( (SPI3->SR ) & ( SPI_FLAG_RXP) )!=0)
{
//Save the RX data
ArrGenRx[IndRx]=*p_RXDR_SPI3;
IndRx++;
ArrGenRx[IndRx]=*p_RXDR_SPI3;
IndRx++;
Len_Data=Len_Data-2;
//End Msg ?
if(Len_Data==0)
{
Len_Data=24;
...
IndRx=0;
IndTx=0;
}
else
{
//Load data to be TX; normally comes from a Array, but for simplify
//i send costant
*p_TXDR_SPI3=0xAA;
IndTx++;
*p_TXDR_SPI3=0xBB;
IndTx++;
}
}//RXP INT ??
}
Also changing the MISO pin, nothing change.
Thanks for any help
Roberto