SPI_multiple_bytes_transfer
I am sending multiple bytes in spi protocol. The sender is sending properly through AARDWARK(Total Phase Control)Software. But only the odd number of bytes are received and the receiving is not proper using these HAL_Functions. What is the issue?check the following logic and help me if you could
int main(void) {
SystemClock_Config();
MX_GPIO_Init();
MX_SPI3_Init();
MX_LPUART1_UART_Init();
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_12, GPIO_PIN_SET);
/*
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_SPI_TransmitReceive(&hspi3, data_tra, data_rec, 5, HAL_MAX_DELAY);
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_12, GPIO_PIN_SET);
*/
/*
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_SPI_TransmitReceive_IT(&hspi3, data_tra, data_rec, 3);
HAL_Delay(1);
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_12, GPIO_PIN_SET);
*/
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi3, data_tra, 3, HAL_MAX_DELAY);
HAL_SPI_Receive(&hspi3, data_rec, 3, HAL_MAX_DELAY);
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_12, GPIO_PIN_SET);
while (1) {
}
}