SPI Transmit and Receive in STM32F207ZGT6
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_SPI1_Init();
MX_USART3_UART_Init();
/* USER CODE BEGIN 2 */
----> HAL_SPI_Receive_IT(&hspi1, (uint8_t*) &rx_data, sizeof(rx_data));
/* USER CODE END 2 */
while (1)
{
HAL_SPI_Transmit(&hspi1, (uint8_t*) &test,sizeof(test), HAL_MAX_DELAY);
delay(10000);
}
}
I use SPI1 module in FullDuplexMaster Mode.
I use interrupt to receive data from the SPI Slave.
The Thing is that if I add the Line which is arrowed--->HAL_SPI_Receive_IT(), the sending is not happening.
I want to know why this is happening. help me why?
Thank You