Skip to main content
Graduate
May 18, 2024
Question

SPI TransmitReceive wrong behavior

  • May 18, 2024
  • 3 replies
  • 2361 views

Hello ST expert.

I'm trying to create SPI communication as shown in the CubeMX image.

Paulo971_0-1716058239690.png

Paulo971_1-1716058254335.png

and the following code

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <stdio.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
SPI_HandleTypeDef hspi3;

TIM_HandleTypeDef htim1;
TIM_HandleTypeDef htim2;
TIM_HandleTypeDef htim3;
TIM_HandleTypeDef htim4;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_TIM1_Init(void);
static void MX_TIM2_Init(void);
static void MX_TIM3_Init(void);
static void MX_TIM4_Init(void);
static void MX_SPI3_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint8_t spi_buf_tx[4] = {90, 00, 00, 00};
uint8_t spi_buf_rx[4];
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
	uint16_t duty_cycle = 0;

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_TIM1_Init();
 MX_TIM2_Init();
 MX_TIM3_Init();
 MX_TIM4_Init();
 MX_SPI3_Init();
 /* USER CODE BEGIN 2 */

 TIM1->CCR1 = duty_cycle;
 HAL_TIM_Base_Start(&htim1); // activation du timer (optionel)
 HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1); //PWM start
 HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1); //PWM start
 HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_1); //PWM start
 HAL_TIM_PWM_Start(&htim4, TIM_CHANNEL_1); //PWM start

 HAL_SPI_TransmitReceive(&hspi3, spi_buf_tx, spi_buf_rx, 4, 100);
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {

 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 84;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief SPI3 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_SPI3_Init(void)
{

 /* USER CODE BEGIN SPI3_Init 0 */

 /* USER CODE END SPI3_Init 0 */

 /* USER CODE BEGIN SPI3_Init 1 */

 /* USER CODE END SPI3_Init 1 */
 /* SPI3 parameter configuration*/
 hspi3.Instance = SPI3;
 hspi3.Init.Mode = SPI_MODE_MASTER;
 hspi3.Init.Direction = SPI_DIRECTION_2LINES;
 hspi3.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi3.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi3.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi3.Init.NSS = SPI_NSS_SOFT;
 hspi3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
 hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi3.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi3.Init.CRCPolynomial = 10;
 if (HAL_SPI_Init(&hspi3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN SPI3_Init 2 */

 /* USER CODE END SPI3_Init 2 */

}

/**
 * @brief TIM1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM1_Init(void)
{

 /* USER CODE BEGIN TIM1_Init 0 */

 /* USER CODE END TIM1_Init 0 */

 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};
 TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};

 /* USER CODE BEGIN TIM1_Init 1 */

 /* USER CODE END TIM1_Init 1 */
 htim1.Instance = TIM1;
 htim1.Init.Prescaler = 8-1;
 htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim1.Init.Period = 65535-1;
 htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim1.Init.RepetitionCounter = 0;
 htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = 800;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
 sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
 if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
 sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
 sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
 sBreakDeadTimeConfig.DeadTime = 0;
 sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
 sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
 sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
 if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM1_Init 2 */

 /* USER CODE END TIM1_Init 2 */
 HAL_TIM_MspPostInit(&htim1);

}

/**
 * @brief TIM2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM2_Init(void)
{

 /* USER CODE BEGIN TIM2_Init 0 */

 /* USER CODE END TIM2_Init 0 */

 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};

 /* USER CODE BEGIN TIM2_Init 1 */

 /* USER CODE END TIM2_Init 1 */
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 0;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 4294967295;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_PWM_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM2_Init 2 */

 /* USER CODE END TIM2_Init 2 */
 HAL_TIM_MspPostInit(&htim2);

}

/**
 * @brief TIM3 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM3_Init(void)
{

 /* USER CODE BEGIN TIM3_Init 0 */

 /* USER CODE END TIM3_Init 0 */

 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};

 /* USER CODE BEGIN TIM3_Init 1 */

 /* USER CODE END TIM3_Init 1 */
 htim3.Instance = TIM3;
 htim3.Init.Prescaler = 0;
 htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim3.Init.Period = 65535;
 htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim3) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_PWM_Init(&htim3) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM3_Init 2 */

 /* USER CODE END TIM3_Init 2 */
 HAL_TIM_MspPostInit(&htim3);

}

/**
 * @brief TIM4 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM4_Init(void)
{

 /* USER CODE BEGIN TIM4_Init 0 */

 /* USER CODE END TIM4_Init 0 */

 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};

 /* USER CODE BEGIN TIM4_Init 1 */

 /* USER CODE END TIM4_Init 1 */
 htim4.Instance = TIM4;
 htim4.Init.Prescaler = 0;
 htim4.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim4.Init.Period = 65535;
 htim4.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim4.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim4) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim4, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_PWM_Init(&htim4) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim4, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 if (HAL_TIM_PWM_ConfigChannel(&htim4, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM4_Init 2 */

 /* USER CODE END TIM4_Init 2 */
 HAL_TIM_MspPostInit(&htim4);

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOC, FR_2_Pin|FR_1_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(FR_3_GPIO_Port, FR_3_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(SPI3_CS_GPIO_Port, SPI3_CS_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(FR_4_GPIO_Port, FR_4_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pins : FR_2_Pin FR_1_Pin */
 GPIO_InitStruct.Pin = FR_2_Pin|FR_1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /*Configure GPIO pins : FG_2_Pin FG_1_Pin */
 GPIO_InitStruct.Pin = FG_2_Pin|FG_1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /*Configure GPIO pin : FR_3_Pin */
 GPIO_InitStruct.Pin = FR_3_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(FR_3_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : FG_3_Pin */
 GPIO_InitStruct.Pin = FG_3_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(FG_3_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : SPI3_CS_Pin */
 GPIO_InitStruct.Pin = SPI3_CS_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(SPI3_CS_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : FR_4_Pin */
 GPIO_InitStruct.Pin = FR_4_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(FR_4_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : FG_4_Pin */
 GPIO_InitStruct.Pin = FG_4_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(FG_4_GPIO_Port, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

Normally with the HAL_SPI_TransmitReceive function I should receive on my spi_buf_rx the same thing as spi_buf_tx but instead I receive 255 as shown in the debugging session.

Paulo971_2-1716058418846.png

What have I done wrong?

Best regard.

Paulo971

    This topic has been closed for replies.

    3 replies

    Graduate II
    May 18, 2024

    @Paulo971 wrote:

    ...

    Normally with the HAL_SPI_TransmitReceive function I should receive on my spi_buf_rx the same thing as spi_buf_tx but instead I receive 255 as shown in the debugging session.

    ...


    What makes you believe this?

    Did you have your "debugging session" displaying the buffers when you ran your code?

    Have you examined the SPI signals with a scope or logic analyzer?

    Paulo971Author
    Graduate
    May 18, 2024

    the last screenshot is my debugging session which shows me that I have two different things.

    I followed the tutorial below and it shows that there is exactly the same thing for the tx and rx buff.

    https://www.youtube.com/watch?v=5MYlSn-wR5g


    I don't have the tools to examine the SPI signal.

    Visitor II
    May 19, 2024

    What I see on your debug session:
    - you send four bytes and you get four bytes (as it should with regular SPI as "full-duplex")
    - you get 0xFF as bytes back on MISO (Rx) (looks like "open" MISO signal or external chip does not respond)

    Why? You have to figure out why:
    - is there a chip connected?
    - are you sending the "right" command ("SPI Protocol"), with correct SPI mode, MSB vs. LSB, clock speed so that the external chip should respond? Is the nCS signal correct and connected? (is your external chip high or low active?)

    If you are not sure if your SPI on MCU works:
    - disconnect the external chip
    - and connect with a flying wire MISO and MOSI: do you see now that all comes back in the same way as you have sent?
    - you can also connect nCS with MISO: you should see all zero (if your nCS is low active)

    If so: your SPI on MCU is fine. Everything else, why you do not get a SPI response from external chip, is related to the "SPI Protocol", how do you talk to the external chip (SPI mode, MSB. vs LSB, coding of SPI bytes, CS behavior (low or high active), SPI clock you use, ...).

    Test it step by step:
    - fill receiver buffer with a pattern - is it overwritten with 0xFF - then you get 0xFF on MISO
    - verify if nCS, SPI mode, MSB vs. LSB, SPI clock speed are correct
    - verify that you send the right coding for a command, the right length for a transaction, right parameters
    - verify that your external chip is powered, out of reset
    - verify if you have to send a specific command first, e.g. to bring chip form deep sleep to active mode

    Most of the time: I try to read the Chip ID via SPI from an external chip. If I do not get a reasonable response, telling me the correct/expected ChipID - I do not keep going to use or configure the chip.
    If the chip does not have a ChipID: go to datasheet and see if you can find a register with reset defaults which are not all bits 0 or 1, e.g. a value not 0 or 0xFF: try to read this register. If you get it correctly - your SPI and "SPI protocol" is correct.

    If all this does not work - it does not make sense to keep going. The basics have to work first.

    Visitor II
    May 20, 2024

    You used the NSS(CS) pin as standard GPIO (Software NSS Signal).
    You have to control the NSS(CS) pin by Software.

    static void MX_SPI3_Init(void)
    {
     hspi3.Init.NSS = SPI_NSS_SOFT; // Software NSS Signal
    }
    
    static void MX_GPIO_Init(void)
    {
     /*Configure GPIO pin Output Level */
     HAL_GPIO_WritePin(SPI3_CS_GPIO_Port, SPI3_CS_Pin, GPIO_PIN_SET); // CS = High
    }
    
    int main(void)
    {
     HAL_GPIO_WritePin(SPI3_CS_GPIO_Port, SPI3_CS_Pin, GPIO_PIN_RESET); // CS = Low
     HAL_SPI_TransmitReceive(&hspi3, spi_buf_tx, spi_buf_rx, 4, 100);
     HAL_GPIO_WritePin(SPI3_CS_GPIO_Port, SPI3_CS_Pin, GPIO_PIN_SET); // CS = High
    }
    Graduate II
    May 20, 2024

    SPI3 is the Master and since NSS is configured as software the SPI module doesn't care about it.  The CS signal is only for the Slave's benefit in this case - he'll get a SPI clock and MOSI driven even without a CS assertion.

    Paulo971Author
    Graduate
    May 22, 2024

    Please find the diagram showing how my BLE module (Adafruit Bluefruit LE SPI Friend) and my MCU are connected.

    Paulo971_0-1716385352780.png

    Paulo971_1-1716385382830.png

    I need to receive data from the BLE module and send data from the MCU.

    I've changed the prescaler to 16, checked the cables and so far I've used the function ‘HAL_SPI_Receive(&hspi3, spi_buf_rx, sizeof(spi_buf_rx), 1000)’ but I still can't receive any data.

    Paulo971_2-1716387041138.png

     

     

    Graduate II
    May 22, 2024

    Disconnect MOSI and MISO from the BLE module.

    Connect MOSI and MISO at the MCU.

    Run your test.  You should see the same data received as transmitted.  If not, your configuration of the SPI is likely incorrect.  If it's the same, disconnect MOSI and MISO from each other and reconnect to the BLE module.  Then research the SPI protocol of the BLE module and implement that in your code.