Skip to main content
Graduate
November 8, 2024
Solved

SRAM internal frame Buffer - LTDC - Strange Issue

  • November 8, 2024
  • 1 reply
  • 1111 views

hi,

I have successfully connected LTDC display(480x272) with STM32H723ZGT6 - RGB565 mode .

I could able to image file from internal Flash Memory .

MMARI1_0-1731035396898.jpeg

I could able to Load Perfect colour from DMA2D by using. framebuffer in global level .

uint16_t framebuffer[480*272];

 

HAL_DMA2D_Start(&hdma2d, 0x000FF000,(uint32_t)framebuffer, 480, 272);
HAL_DMA2D_PollForTransfer(&hdma2d, 10);

 

I could not able to transfer colour from SRAM to LTDC by using .

for (int y=0; y<272; y++)
 {
 for (int x=0; x<480; x++)
 	 {
 	 framebuffer[y*480 + x] = 0xF800;
 	 }
 }

 

MMARI1_2-1731035769630.jpeg

Erratic fill Screen happening when i transfer data to frame buffer memory . Even i reduced the speed of LTDC and total clock but nothing worked out .

DMA2D using same frame buffer memory and transferring register to Memory and working fine .

    This topic has been closed for replies.
    Best answer by MM..1

    Primary change two lines to by address mode :

     

    //uint16_t framebuffer[480*272];
    #define FBUF 0x... //reserved memory add start in Dx must be alligned for ltdc limits
    ...
    pLayerCfg.FBStartAdress = (uint32_t)FBUF;

     

    and in linker script setup RAM areas and sizes .

    But when DMA2D into actual buf works, then maybe other mistake in your config. Check MPU and optimize level can remove your code , because filled p_buf is never used... change it to framebuffer and declare volatile.

    1 reply

    ST Employee
    November 8, 2024

    Hello @MMARI.1 ,

    could you please share your code as this description is not clear to me.

    I could not able to transfer color from SRAM to LTDC by using.

    for (int y=0; y<272; y++)
     {
     for (int x=0; x<480; x++)
     	 {
     	 framebuffer[y*480 + x] = 0xF800;
     	 }
     }

    in this case is the frame buffer declared in SRAM ?

    also, I would recommend you check 4861 section 7.2.5.
    Regards

    MMARI.1Author
    Graduate
    November 10, 2024

     

    How to separate the SRAM- d1 exclusive for LTDC frame buffer . how  i can directly assign the SRAM address in the LTDC Frame buffer setting . 255kb size required for frame buffer  . i can't assign the staring address the of SRAM- D1 because   mcu using some initialization data's . what should i have to include and modify in the linker file for Dividing the SRAM-D1 in to 2 .? 

    /* USER CODE BEGIN Header */
    /**
     ******************************************************************************
     * @file : main.c
     * @brief : Main program body
     ******************************************************************************
     * @attention
     *
     * Copyright (c) 2024 STMicroelectronics.
     * All rights reserved.
     *
     * This software is licensed under terms that can be found in the LICENSE file
     * in the root directory of this software component.
     * If no LICENSE file comes with this software, it is provided AS-IS.
     *
     ******************************************************************************
     */
    /* USER CODE END Header */
    /* Includes ------------------------------------------------------------------*/
    #include "main.h"
    
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN PTD */
    
    /* USER CODE END PTD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    
    DMA2D_HandleTypeDef hdma2d;
    
    LTDC_HandleTypeDef hltdc;
    
    /* USER CODE BEGIN PV */
    
    uint16_t framebuffer[480*272];
    
    //(uint32_t)&framebuffer;
    
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    static void MPU_Config(void);
    static void MX_GPIO_Init(void);
    static void MX_DMA2D_Init(void);
    static void MX_LTDC_Init(void);
    /* USER CODE BEGIN PFP */
    
    /* USER CODE END PFP */
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    
    /* USER CODE END 0 */
    
    /**
     * @brief The application entry point.
     * @retval int
     */
    int main(void)
    {
    
     /* USER CODE BEGIN 1 */
    
     /* USER CODE END 1 */
    
     /* MPU Configuration--------------------------------------------------------*/
     MPU_Config();
    
     /* Enable the CPU Cache */
    
     /* Enable I-Cache---------------------------------------------------------*/
     SCB_EnableICache();
    
     /* Enable D-Cache---------------------------------------------------------*/
     SCB_EnableDCache();
    
     /* MCU Configuration--------------------------------------------------------*/
    
     /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
     HAL_Init();
    
     /* USER CODE BEGIN Init */
    
     /* USER CODE END Init */
    
     /* Configure the system clock */
     SystemClock_Config();
    
     /* USER CODE BEGIN SysInit */
    
     /* USER CODE END SysInit */
    
     /* Initialize all configured peripherals */
     MX_GPIO_Init();
     MX_DMA2D_Init();
     MX_LTDC_Init();
     /* USER CODE BEGIN 2 */
    
     /* USER CODE END 2 */
    
     /* Infinite loop */
     /* USER CODE BEGIN WHILE */
     while (1)
     {
     /* USER CODE END WHILE */
    
     /* USER CODE BEGIN 3 */
    	 uint16_t *p_buf = framebuffer;
    	 uint16_t color_tbl[3] = {0xF800, 0x07E0, 0x001F};
    	 uint16_t color;
    	 static uint8_t index = 0;
    	 color = color_tbl[index];
    	 index = (index + 1) % 3;
    	 for (int y=0; y<272; y++)
    	 {
    	 for (int x=0; x<480; x++)
    	 {
    	 p_buf[y*480 + x] = color;
    	 }
    	 }
    	 HAL_Delay(1500);
     }
     /* USER CODE END 3 */
    }
    
    /**
     * @brief System Clock Configuration
     * @retval None
     */
    void SystemClock_Config(void)
    {
     RCC_OscInitTypeDef RCC_OscInitStruct = {0};
     RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
     /** Supply configuration update enable
     */
     HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
    
     /** Configure the main internal regulator output voltage
     */
     __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
    
     while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
    
     /** Initializes the RCC Oscillators according to the specified parameters
     * in the RCC_OscInitTypeDef structure.
     */
     RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
     RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
     RCC_OscInitStruct.HSICalibrationValue = 64;
     RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
     RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
     RCC_OscInitStruct.PLL.PLLM = 4;
     RCC_OscInitStruct.PLL.PLLN = 34;
     RCC_OscInitStruct.PLL.PLLP = 1;
     RCC_OscInitStruct.PLL.PLLQ = 2;
     RCC_OscInitStruct.PLL.PLLR = 2;
     RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
     RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
     RCC_OscInitStruct.PLL.PLLFRACN = 3072;
     if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Initializes the CPU, AHB and APB buses clocks
     */
     RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
     |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
     |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
     RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
     RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
     RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
     RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
     RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
     RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
     RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
    
     if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
     {
     Error_Handler();
     }
    }
    
    /**
     * @brief DMA2D Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_DMA2D_Init(void)
    {
    
     /* USER CODE BEGIN DMA2D_Init 0 */
    
     /* USER CODE END DMA2D_Init 0 */
    
     /* USER CODE BEGIN DMA2D_Init 1 */
    
     /* USER CODE END DMA2D_Init 1 */
     hdma2d.Instance = DMA2D;
     hdma2d.Init.Mode = DMA2D_R2M;
     hdma2d.Init.ColorMode = DMA2D_OUTPUT_RGB565;
     hdma2d.Init.OutputOffset = 0;
     if (HAL_DMA2D_Init(&hdma2d) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN DMA2D_Init 2 */
    
     /* USER CODE END DMA2D_Init 2 */
    
    }
    
    /**
     * @brief LTDC Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_LTDC_Init(void)
    {
    
     /* USER CODE BEGIN LTDC_Init 0 */
    
     /* USER CODE END LTDC_Init 0 */
    
     LTDC_LayerCfgTypeDef pLayerCfg = {0};
    
     /* USER CODE BEGIN LTDC_Init 1 */
    
     /* USER CODE END LTDC_Init 1 */
     hltdc.Instance = LTDC;
     hltdc.Init.HSPolarity = LTDC_HSPOLARITY_AL;
     hltdc.Init.VSPolarity = LTDC_VSPOLARITY_AL;
     hltdc.Init.DEPolarity = LTDC_DEPOLARITY_AL;
     hltdc.Init.PCPolarity = LTDC_PCPOLARITY_IPC;
     hltdc.Init.HorizontalSync = 3;
     hltdc.Init.VerticalSync = 3;
     hltdc.Init.AccumulatedHBP = 46;
     hltdc.Init.AccumulatedVBP = 15;
     hltdc.Init.AccumulatedActiveW = 526;
     hltdc.Init.AccumulatedActiveH = 287;
     hltdc.Init.TotalWidth = 534;
     hltdc.Init.TotalHeigh = 295;
     hltdc.Init.Backcolor.Blue = 0;
     hltdc.Init.Backcolor.Green = 0;
     hltdc.Init.Backcolor.Red = 0;
     if (HAL_LTDC_Init(&hltdc) != HAL_OK)
     {
     Error_Handler();
     }
     pLayerCfg.WindowX0 = 0;
     pLayerCfg.WindowX1 = 480;
     pLayerCfg.WindowY0 = 0;
     pLayerCfg.WindowY1 = 272;
     pLayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_RGB565;
     pLayerCfg.Alpha = 255;
     pLayerCfg.Alpha0 = 255;
     pLayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_CA;
     pLayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_CA;
     pLayerCfg.FBStartAdress = (uint32_t)&framebuffer;
     pLayerCfg.ImageWidth = 480;
     pLayerCfg.ImageHeight = 272;
     pLayerCfg.Backcolor.Blue = 0;
     pLayerCfg.Backcolor.Green = 0;
     pLayerCfg.Backcolor.Red = 0;
     if (HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN LTDC_Init 2 */
    
     /* USER CODE END LTDC_Init 2 */
    
    }
    
    /**
     * @brief GPIO Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_GPIO_Init(void)
    {
     GPIO_InitTypeDef GPIO_InitStruct = {0};
    /* USER CODE BEGIN MX_GPIO_Init_1 */
    /* USER CODE END MX_GPIO_Init_1 */
    
     /* GPIO Ports Clock Enable */
     __HAL_RCC_GPIOF_CLK_ENABLE();
     __HAL_RCC_GPIOC_CLK_ENABLE();
     __HAL_RCC_GPIOA_CLK_ENABLE();
     __HAL_RCC_GPIOB_CLK_ENABLE();
     __HAL_RCC_GPIOD_CLK_ENABLE();
    
     /*Configure GPIO pin Output Level */
     HAL_GPIO_WritePin(GPIOB, GPIO_PIN_8, GPIO_PIN_SET);
    
     /*Configure GPIO pin : PB8 */
     GPIO_InitStruct.Pin = GPIO_PIN_8;
     GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
     GPIO_InitStruct.Pull = GPIO_NOPULL;
     GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
     HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
    
    /* USER CODE BEGIN MX_GPIO_Init_2 */
    /* USER CODE END MX_GPIO_Init_2 */
    }
    
    /* USER CODE BEGIN 4 */
    
    /* USER CODE END 4 */
    
     /* MPU Configuration */
    
    void MPU_Config(void)
    {
     MPU_Region_InitTypeDef MPU_InitStruct = {0};
    
     /* Disables the MPU */
     HAL_MPU_Disable();
    
     /** Initializes and configures the Region and the memory to be protected
     */
     MPU_InitStruct.Enable = MPU_REGION_ENABLE;
     MPU_InitStruct.Number = MPU_REGION_NUMBER0;
     MPU_InitStruct.BaseAddress = 0x0;
     MPU_InitStruct.Size = MPU_REGION_SIZE_4GB;
     MPU_InitStruct.SubRegionDisable = 0x87;
     MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
     MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
     MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
     MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
     MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
     MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
    
     HAL_MPU_ConfigRegion(&MPU_InitStruct);
     /* Enables the MPU */
     HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
    
    }
    
    /**
     * @brief This function is executed in case of error occurrence.
     * @retval None
     */
    void Error_Handler(void)
    {
     /* USER CODE BEGIN Error_Handler_Debug */
     /* User can add his own implementation to report the HAL error return state */
     __disable_irq();
     while (1)
     {
     }
     /* USER CODE END Error_Handler_Debug */
    }
    
    #ifdef USE_FULL_ASSERT
    /**
     * @brief Reports the name of the source file and the source line number
     * where the assert_param error has occurred.
     * @PAram file: pointer to the source file name
     * @PAram line: assert_param error line source number
     * @retval None
     */
    void assert_failed(uint8_t *file, uint32_t line)
    {
     /* USER CODE BEGIN 6 */
     /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
     /* USER CODE END 6 */
    }
    #endif /* USE_FULL_ASSERT */

    MM..1Answer
    Graduate II
    November 10, 2024

    Primary change two lines to by address mode :

     

    //uint16_t framebuffer[480*272];
    #define FBUF 0x... //reserved memory add start in Dx must be alligned for ltdc limits
    ...
    pLayerCfg.FBStartAdress = (uint32_t)FBUF;

     

    and in linker script setup RAM areas and sizes .

    But when DMA2D into actual buf works, then maybe other mistake in your config. Check MPU and optimize level can remove your code , because filled p_buf is never used... change it to framebuffer and declare volatile.