Skip to main content
Visitor II
May 8, 2024
Question

SRM32L4 Firmware Installation

  • May 8, 2024
  • 2 replies
  • 2279 views

Hello

I cannot complete the step 4 of Tools Installation, the installation of STM32CubeL3 Firmware package.

The STM32CubeMX program is not accepting it.

I downloaded it from the st.com website, but the program cannot recognize it.

What do I have to do?

Thanks

    This topic has been closed for replies.

    2 replies

    Graduate II
    May 8, 2024

    ?? SRM32L4, STM32CubeL3, STM32F4 Series

    Which is it?

    Ideally you let STM32 CubeMX pull the files directly. Why can't you do that?

    Alternately you can download the .ZIP from the CubeXX package you need to install "From Local"

    I'd imagine there are YouTube tutorials on this..

    FabioCCAuthor
    Visitor II
    May 8, 2024

    Thanks.

    Yes, I downloaded the zipped archive.

    Now, how to install it "from local"?

    Technical Moderator
    May 8, 2024

    On the STM32MCU Cube packages click on the button "From Local..." of this figure:

    Stepbystep_Download_STM32CubeL4.png

    And follow the instructions.

    Best Regards.

    STTwo-32 

    FabioCCAuthor
    Visitor II
    May 9, 2024

    Clicked on it, more than 10 minutes ago, in the same program section you are showing in the picture.. Nothing is happening.