Standby mode on stmL433 drawing too much current
Hi
I have a a stm32L433 48 pin processor and trying to get it into low power. I am using the STLink-V3PWR module with stm32Cube Monitor Power module. First of all I placed a known value resistor across the STLink-V3PWR to make sure it is reading the correct value, then tried the following:
1. I am using a MIC5219-3.3YM5-TR from the input with the STLink-V3PWR set to 3.6v. And on its own it draws 85uA.
2. I then added all the resistors and capacitors needed and it measured 96uA.
3. I added the STM32L433 and programmed it to first run for approx 5 seconds in normal mode (16MHz), then drop into standby mode. On the output you can see it drop quite a bit, but the lowest current is approx 650uA (far too much current) as you can see on the graph below.

My code is below after 5 seconds of normal operation. I tried HAL_PWREx_EnterSHUTDOWNMode(); without Putting the Ram in Retention, but still the same,
void EnterLowPower()
{
RCC->APB1RSTR1 |= RCC_APB1RSTR1_USBFSRST;
RCC->APB1RSTR1 &= ~RCC_APB1RSTR1_USBFSRST;
RCC->APB1ENR1 &= ~RCC_APB1ENR1_USBFSEN;
__HAL_RCC_GPIOA_CLK_DISABLE();
__HAL_RCC_GPIOB_CLK_DISABLE();
__HAL_RCC_GPIOC_CLK_DISABLE();
__HAL_RCC_GPIOD_CLK_DISABLE();
HAL_PWREx_EnableSRAM2ContentRetention();
HAL_PWR_EnterSTANDBYMode();
}
Any suggestions what I am doing wrong?
Many thanks in advance
Scott