stlink v3 mini cannot program c031g4u6, Target no device found
i am sorry for creating a lot of post recently but i just can not program my microcontrollers.
when ever i try to program it i get this:
STMicroelectronics ST-LINK GDB server. Version 7.5.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
i have a stlink v3 mini and 3 stm32c031g4u6 microcontrollers soldered to proper breakout boards.
i have SWD interface soldered from the edge connector because i had no luck with cn4.
SWDIO, SWCLK and RESET are connected. i also have an led soldered to power pins to be sure its powered.
i am sure of the soldering job.
on my first post someone recommeded i solder capasitors so i did that still no result.
i am using linux mint's latest and the code i am trying to upload is just empty machine generated code
here are the pics:





i made a breakout for cn4:

sorry for the bad solder job
thanks for help