STLINK-V3MINIE connecting SWO and VCP_TX pins
I am making an adapter between 6‐pin target debug header and 14-pin STDC14 connector. The same cable will be used to program and debug both M0+ and M4 targets.
Can I hard-wire SWO (pin 8 ) and T_VCP_TX (pin 14) together? The idea is to have an option on target board to use either UART or SWO, whatever is available.
Will UART transmission affect SWD functionality by sending garbage (from SWV standpoint) to SWO pin?
update: sorry, posted this into wrong forum. can someone can move this into "dev tools", please?
update 2: I think I found an answer here: https://community.st.com/t5/stm32-mcus-boards-and-hardware/uart-signal-on-swo-pin-from-st-link-v2-3/m-p/742773/highlight/true#M22581