STM32 Interleaved ADC Sample Timestamping
Hi, I am using STM32L476RG-Nucleo64 boards for one of my ultrasound projects. Basically, the process is:
1)Send 2MHz pulses with pwm
2) Sample 1000points with 8-bit interleaved ADC(500 each) and DMA
3) Send ADC data through SPI.
4) Wait TIM3 to trigger again for both ADC and PWM and back to 1
Everything is working fine, only problem is that I need the time label of each sample -Or somehow calculate the Δt between them- in ADC so that I can identify the Δt of some peaks positions in the data but it is troubling me because of maxed ADC speed
I made ADC interleaved, 8-bit and 2.5 cycles to work at max speed, not like a timer-triggered ADC. Therefore I cannot measure the total 1000 sampling time for dividing by 1000 (Not sure if all samplings are done with same speed tho).
I tried to measure the time using DMA callback and ADC callback using DWT but it is saying that the time is around 35ms and I know it is wrong because I can confirm with an oscilloscope that the data window I am sampling with 1000 sampling is around 60us.
You can review the stm32 main.c from here: main.c
Note: In the code I enabled ContiniousConvMode even though it is not recommended for triggered ADC but somehow my version works with continious mode enabled and stops working when it is disabled.
Also -Maybe I am misinterpreting some concepts- but my real sampling rate seems to be a lot higher than my calculations. I set 8-bit ADC interleaved with 2.5 sampling cycle and 2 cycle delay, which should give 16 cycle for 2ADC which is 10MHz sampling rate with 80MHz clock. With this setup 100 samples should take 10us, but when I compare this with an oscilloscope, 10us difference is 150 samples which is 1.5x higher than it should be.