STM32 internal oscillator drift over time
I designed a board using a STM32L031F6P6 about 4 years ago, (April 2021). The design has been using the internal oscillator running at 16Mhz perfectly for years. Then this past summer all of a sudden the RS232 Uart stopped receiving data until I cycle the power on the unit. The problem has now become more frequent, and the Tx on the uart is also bad, so it appears like the baud rate is bad, which means the internal oscillator is drifting. My spi bus remains 100% fine btw.
Has anyone ever seen this with the internal oscillators?, can they drift over time like this . I would expect the accuracy of the oscillator to be stable .
Thanks .