STM32 MCU Choosing and programming
Hello everyone!
After some more studying on STM32 ecosystem and how the programming of those boards work I've come to a blunder:
I am designing a project with an STM32 Microcontroller that I need to program (of course), and I don't know what method should I use. Initially I thought it would be perfect to go with the USB, but then I realised that the development board that I used to program via plug'n'play USB (where the idea of USB programming came), has an ST-Link debugger included that allowed me to do so.
This means that I either have to include a debugger in my schematic and PCB design (more space, more components, bigger board etc), or buy a separate one and get the JTAG/SWD pins out with a connector. I also understand that with BOOT0 hooked to power, via a switch, the MCU is programmable with USB, but I don't understand what other tools do I need to make the USB programming possible.....
1. What is the best way to have a smooth programming experience with my board (it might need several trial and error with the code until its working and complete - I am also a noobie regarding the STM32 programming)?
Regarding the MCU model, initially I chose STM32F103, but some guy told me it's quite primitive and has no DFU which makes it harder to program/debug via USB. In the past I worked with STM32L010RB dev board, maybe I should switch to that one??? My application is about measuring some currents and transferring the values to my PC - the values are transferred via I2C to the MCU, and we are talking about 46 measurements values that are in the form of Voltage and corresponding current. It is USB-powered.
2.What MCU should I choose??
3. Can someone enlighten me on this path of working with and STM32 on a more advanced manner than "dev board light the LED blink blink"??