STM32 Not Detected via ST-Link V2 – Voltage Detected but No Connection
Hi everyone,
I'm having trouble flashing my STM32 microcontroller using an ST-Link V2. STM32CubeProgrammer detects the target voltage, but it fails to connect to the MCU. Here's a summary of my setup and what I've tried:
Setup:
Microcontroller: STM32H723ZGT6
ST-Link Version: ST-Link V2
Flashing Tool: STM32CubeProgrammer (latest version)
Connection Interface: SWD
Target Voltage Detected: 3.12 V
What I’ve Tried:
Verified SWD wiring (SWDIO, SWCLK, GND, VCC)
BOOT0 set to 0 (boot from flash)
Checked for power on the board
Question:
What else should I try to get the MCU detected? Could this be a clone ST-Link V2 issue, or something else with my MCU or wiring?
Any help is appreciated — thank you!