Question
STM32 part with the most avialable rotary/quadrature encoder inputs
Let me start by saying:
- Yes I know the STM32 Finder exists, no it doesn't help me find what I need
- Yes I've seen this thread but I do not want to get into manually coding a script to try and find parts if I can avoid it
- Yes I have used the CubeMX and no it can't filter for this requirement
Basically I'm after an STM32 that will allow me to interface the maximum number of rotary encoders possible into timer inputs (no I do not want to bit-bang it).
That's it - any suggestions welcome!