Skip to main content
Visitor II
November 18, 2024
Question

STM32_Programmer_CLI fails to flash

  • November 18, 2024
  • 1 reply
  • 443 views

Using the STM32 CLI on Windows:

STM32_Programmer_CLI.exe c port=swd reset=HWrst -e all -d my_filename.hex -v -s -g

 

This just prints:

JBill10_0-1731965731898.png

 

If I remove the -d option, it performs the erase, so I know it can talk to the chip.  I have tried the verbosity options, they do not print any additional output.

All features work fine on Linux, using the same hardware.  It looks like a bug with the Windows build of the CLI.

 

 

    This topic has been closed for replies.

    1 reply

    JBill.10Author
    Visitor II
    November 18, 2024

    This bug is present in 2.16.0 as well.

    I also tried 2.15.0, which doesn't even print the banner, it just immediately crashes.