Skip to main content
Explorer
March 2, 2024
Question

stm32 timer doesn't count

  • March 2, 2024
  • 2 replies
  • 3157 views

hi, i have a problem with my stm32 timer in counter mode, i connected it to a lcd screen, and put a pulse signal in pin PB0, and i wanted to count these pulses and show them on the lcd, but the pulse count is stuck at 0, can you help me with it please? i think it's the timer configuration or the interrupt problem but i'm not sure, and thanks in advance.

 

    This topic has been closed for replies.

    2 replies

    Graduate
    March 2, 2024

    Isolate the problem using breakpoints in Debug single step mode. For example:

    Is the pulse being received?

    Does the interrupt happen?

    Is the correct value being sent to the display?

     

     

    medraoufAuthor
    Explorer
    March 2, 2024

    can you tell me how to do that exactly? it's my first time with it, and i am using a proteus simulation...

    Graduate
    March 2, 2024

    I have no experience with proteus.

     

    Graduate II
    March 2, 2024

    Perhaps you can look in the CubeF1 / HAL example trees for "External Count"

    >>i think it's the timer configuration or the interrupt problem but i'm not sure..

    We could imagine, or you can show the code as you have it so far.

    Post to Github, or use the code pasting tool </>

     

    medraoufAuthor
    Explorer
    March 2, 2024
    /* USER CODE BEGIN Header */
    /* USER CODE END Header */
    /* Includes ------------------------------------------------------------------*/
    #include "main.h"
    #include "lcd8.h"
    volatile uint32_t pulseCount = 0;
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN PTD */
    /* USER CODE END PTD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    TIM_HandleTypeDef htim2;
    
    /* USER CODE BEGIN PV */
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    static void MX_GPIO_Init(void);
    static void MX_TIM2_Init(void);
    /* USER CODE BEGIN PFP */
    /* USER CODE END PFP */
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    /* USER CODE END 0 */
    
    /**
     * @brief The application entry point.
     * @retval int
     */
    int main(void)
    {
     /* USER CODE BEGIN 1 */
     /* USER CODE END 1 */
    
     /* MCU Configuration--------------------------------------------------------*/
    
     /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
     HAL_Init();
    
     /* USER CODE BEGIN Init */
     /* USER CODE END Init */
    
     /* Configure the system clock */
     SystemClock_Config();
    
     /* USER CODE BEGIN SysInit */
     /* USER CODE END SysInit */
    
     /* Initialize all configured peripherals */
     MX_GPIO_Init();
     MX_TIM2_Init();
     /* USER CODE BEGIN 2 */
    
     lcdSetup(GPIOA, GPIO_PIN_8, GPIO_PIN_9, GPIO_PIN_0, GPIO_PIN_1, GPIO_PIN_2, GPIO_PIN_3, GPIO_PIN_4, GPIO_PIN_5, GPIO_PIN_6, GPIO_PIN_7);
     lcdInit();
     HAL_TIM_IC_Start_IT(&htim2, TIM_CHANNEL_1);
     /* USER CODE END 2 */
    
     /* Infinite loop */
     /* USER CODE BEGIN WHILE */
     while (1)
     {
     lcdSetCursor(0, 0);
     lcdWriteInt("Pulses: %d", pulseCount);
     HAL_Delay(1000); // Update LCD every second
     }
     /* USER CODE END WHILE */
    
     /* USER CODE BEGIN 3 */
     /* USER CODE END 3 */
    }
    
    /**
     * @brief System Clock Configuration
     * @retval None
     */
    void SystemClock_Config(void)
    {
     RCC_OscInitTypeDef RCC_OscInitStruct = {0};
     RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
     /** Initializes the RCC Oscillators according to the specified parameters
     * in the RCC_OscInitTypeDef structure.
     */
     RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
     RCC_OscInitStruct.HSIState = RCC_HSI_ON;
     RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
     RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
     RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI_DIV2;
     RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;
     if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Initializes the CPU, AHB and APB buses clocks
     */
     RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
     |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
     RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
     RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
     RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
     RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
    
     if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
     {
     Error_Handler();
     }
    }
    
    /**
     * @brief TIM2 Initialization Function
     * @PAram None
     * @retval None
     */
    void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)
    {
     if (htim->Instance == TIM2)
     {
     pulseCount++; // Increment the pulse count on each capture event
     }
    }
    static void MX_TIM2_Init(void)
    {
    
     /* USER CODE BEGIN TIM2_Init 0 */
     /* USER CODE END TIM2_Init 0 */
    
     TIM_ClockConfigTypeDef sClockSourceConfig = {0};
     TIM_SlaveConfigTypeDef sSlaveConfig = {0};
     TIM_MasterConfigTypeDef sMasterConfig = {0};
     TIM_IC_InitTypeDef sConfigIC = {0};
    
     /* USER CODE BEGIN TIM2_Init 1 */
     /* USER CODE END TIM2_Init 1 */
     htim2.Instance = TIM2;
     htim2.Init.Prescaler = 999;
     htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
     htim2.Init.Period = 65535;
     htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
     htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
     if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
     {
     Error_Handler();
     }
     sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
     if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_TIM_IC_Init(&htim2) != HAL_OK)
     {
     Error_Handler();
     }
     sSlaveConfig.SlaveMode = TIM_SLAVEMODE_DISABLE;
     sSlaveConfig.InputTrigger = TIM_TS_ITR0;
     if (HAL_TIM_SlaveConfigSynchro(&htim2, &sSlaveConfig) != HAL_OK)
     {
     Error_Handler();
     }
     sMasterConfig.MasterOutputTrigger = TIM_TRGO_ENABLE;
     sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;
     if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
     {
     Error_Handler();
     }
     sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;
     sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;
     sConfigIC.ICPrescaler = TIM_ICPSC_DIV2;
     sConfigIC.ICFilter = 0x0;
     if (HAL_TIM_IC_ConfigChannel(&htim2, &sConfigIC, TIM_CHANNEL_1) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN TIM2_Init 2 */
     /* USER CODE END TIM2_Init 2 */
    
    }
    
    /**
     * @brief GPIO Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_GPIO_Init(void)
    {
     GPIO_InitTypeDef GPIO_InitStruct = {0};
    /* USER CODE BEGIN MX_GPIO_Init_1 */
    /* USER CODE END MX_GPIO_Init_1 */
    
     /* GPIO Ports Clock Enable */
     __HAL_RCC_GPIOD_CLK_ENABLE();
     __HAL_RCC_GPIOA_CLK_ENABLE();
     __HAL_RCC_GPIOB_CLK_ENABLE();
    
     /*Configure GPIO pin Output Level */
     HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3
     |GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7
     |GPIO_PIN_8|GPIO_PIN_9, GPIO_PIN_RESET);
    
     /*Configure GPIO pins : PA0 PA1 PA2 PA3
     PA4 PA5 PA6 PA7
     PA8 PA9 */
     GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3
     |GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7
     |GPIO_PIN_8|GPIO_PIN_9;
     GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
     GPIO_InitStruct.Pull = GPIO_NOPULL;
     GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
     HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
    
     /*Configure GPIO pins : PB0 PB3 */
     GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_3;
     GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
     GPIO_InitStruct.Pull = GPIO_PULLUP;
     HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
    
     /*Configure GPIO pins : PB1 PB2 */
     GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_2;
     GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
     GPIO_InitStruct.Pull = GPIO_PULLDOWN;
     HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
    
    /* USER CODE BEGIN MX_GPIO_Init_2 */
    /* USER CODE END MX_GPIO_Init_2 */
    }
    
    /* USER CODE BEGIN 4 */
    /* USER CODE END 4 */
    
    /**
     * @brief This function is executed in case of error occurrence.
     * @retval None
     */
    void Error_Handler(void)
    {
     /* USER CODE BEGIN Error_Handler_Debug */
     /* USER CODE END Error_Handler_Debug */
    }
    
    #ifdef USE_FULL_ASSERT
    /**
     * @brief Reports the name of the source file and the source line number
     * where the assert_param error has occurred.
     * @PAram file: pointer to the source file name
     * @PAram line: assert_param error line source number
     * @retval None
     */
    void assert_failed(uint8_t *file, uint32_t line)
    {
     /* USER CODE BEGIN 6 */
     /* USER CODE END 6 */
    }
    #endif /* USE_FULL_ASSERT */
    ST Employee
    March 4, 2024

    Hello @medraouf

    As you are using an external pin to count the pulses, you need to set the timer input GPIO pin(PB0) in stm32CubeMX (clock source = ETRx) and then enable Timer interrupt in NVIC table, so whenever the counter counts x ticks (defined by ARR), it overflows and generates an interrupt signal!

    In the code, in the counter overflow ISR handler, you can increment your pulsecount variable and write to the LCD. 

    (the callback function’s name that gets called when an overflow interrupt occurs is HAL_TIM_PeriodElapsedCallback) and to start the timer, use HAL_TIM_Base_Start_IT(&htim2);

    Hope that helps!