Skip to main content
Graduate
November 18, 2024
Solved

STM32 UART Byte-to-Byte treatment

  • November 18, 2024
  • 2 replies
  • 1739 views

Hello,

 

I am trying to receive and transmit byte-to-byte on a STM32F429 Discovery, I will be using a STM32U5 Discovery soon. I used UART IT method but maybe there is a better solution...

Objective & Issue:

I want to continuously receive and send byte-to-byte, goal is to apply a function to each byte before transmitting it. Right now I can receive and transmit but I lose some characters in the process.

For example if I send "Passphrase" to Uart using a python script, my implementation will transmit something like "PasPhase". It gets worst if I add more code to do something to the byte for instance...

How can I fix this ? This is not the case if I use a bigger buffer but I want to make sure I receive a byte, treat it and send it through UART ASAP, maybe there is a way to receive next byte at the same time I am treating the current byte ?

 

What I did:

I am using HAL_UART_Receive_IT and HAL_UART_Transmit_IT based on examples I found in the F4 firmware.
I am using a tag UartReady to SET and RESET to alternate between Receive and Transmit.

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define BUFFER_SIZE 1
/* USER CODE END PD */

/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart1;

/* USER CODE BEGIN PV */
__IO ITStatus UartReady = RESET;
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

uint8_t volatile g_aui_read_buf[BUFFER_SIZE] = {0};

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 /* Configure the system clock */
 SystemClock_Config();

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USART1_UART_Init();

 /* Infinite loop */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 UartReady = RESET;
 if (HAL_UART_Receive_IT(&huart1, &g_aui_read_buf, BUFFER_SIZE) != HAL_OK)
 {
 Error_Handler();
 }
 while (UartReady != SET)
 {
 }

 UartReady = RESET;
 if (HAL_UART_Transmit_IT(&huart1, &g_aui_read_buf, BUFFER_SIZE) != HAL_OK)
 {
 Error_Handler();
 }

 while (UartReady != SET)
 {
 }

 /* Reset transmission flag */
 UartReady = RESET;
 }
 /* USER CODE END 3 */
}

/**
 * @brief USART1 Initialization Function
 * None
 * @retval None
 */
static void MX_USART1_UART_Init(void)
{

 huart1.Instance = USART1;
 huart1.Init.BaudRate = 115200;
 huart1.Init.WordLength = UART_WORDLENGTH_8B;
 huart1.Init.StopBits = UART_STOPBITS_1;
 huart1.Init.Parity = UART_PARITY_NONE;
 huart1.Init.Mode = UART_MODE_TX_RX;
 huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart1.Init.OverSampling = UART_OVERSAMPLING_16;
 if (HAL_UART_Init(&huart1) != HAL_OK)
 {
 Error_Handler();
 }
}
/* USER CODE BEGIN 4 */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *p_h_uart)
{
 /* Set transmission flag: transfer complete */
 UartReady = SET;
}
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *p_h_uart)
{
 UartReady = SET;
}

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

 

 

    This topic has been closed for replies.
    Best answer by mƎALLEm

    Example of ring buffer implementation:

    http://www.simplyembedded.org/tutorials/interrupt-free-ring-buffer/

    2 replies

    Super User
    November 18, 2024

    That's a pretty inefficient way of doing it.

    A common approach would be to use a Ring Buffer (aka Circular Buffer): your receiver puts its received characters into the buffer, and your processing takes characters from the buffer.

    Thus the buffer takes up the "slack" between receiving & processing - to prevent data loss.

    mƎALLEmAnswer
    Technical Moderator
    November 18, 2024
    Super User
    November 18, 2024

    @mƎALLEm wrote:

    Example of ring buffer implementation:


    I'm actually using a simplified version of that at the moment!

    @Nero don't be put off by the URL having "interrupt-free" in it: 

    http://www.simplyembedded.org/tutorials/interrupt-free-ring-buffer/

    The article most certainly is about interrupt-driven comms!

    NeroAuthor
    Graduate
    November 19, 2024

    Thank you both @Andrew Neil  @mƎALLEm  for your replies, I will take a look at this !