Skip to main content
Graduate
February 9, 2024
Question

STM32 USB C to UART communication

  • February 9, 2024
  • 2 replies
  • 1449 views

Hello, I am making a development board where I want to use STM32 and USB C connector for power supply to the STM and also for UART communication with the PC. What are the best solutions for this? I looked into using FTDI chip but they are quite expensive. Also, not really sure how to connect the USB C connector for this to work. I am using STM32G0B0CE which has a USB NOE pin which im also not sure how it works or where to connect it.

 

 

Any help or referrals will be welcome

 

 

    This topic has been closed for replies.

    2 replies

    Graduate
    February 9, 2024

    Many STM32 MCUs, including STM32G0Bx, have USB interface onboard, so just use it. I suggest CDC (=VCOM, =UART emulation) as a starting point.

    Super User
    February 9, 2024

    If the UART communication with the PC is only for development, not part of the planned product function - use an external USB to serial chip. There are many of them, much cheaper than FTDI. OTOH the FTDI converter has features not available in cheaper converter.