STM32 VCAP pin problem
Hello,
I have designed a PCB with 3 STM32H725VGT6 MCUs, and assembled them according to my schematic:

(sorry for this resolution, this is from a converted pdf)
All 3 MCUs are the same, from this schematic.
R5 and R2 are just 0R jumpers to select the boot mode.
At first, ST-Link couldn't find any of them. When I checked the voltage on the Vcap pin the MCU1 had 1.0008 V at both 2.2uF caps. STLINK still can't find the target. MCU2 and MCU3 had 0.0000V. on the Vcap pins.
All 3 MCUs have their:
- Orientation in the right place
- VDDA / VREF+ connected
- NRST at high
- 3.3V at all the 100nF decoupling caps
- 2.2uF caps from Murata (ESR < 8 mOhm @ 1 MHz) GRM155R6YA225KE11D
So I was wondering maybe the ICs were bad (which is unlikely considering that they are from Mouser)
I checked the soldering and there were no bridges, but these symptoms are usually caused by some sort of soldering issue. What else should I check?