STM32C0 SDA signal on PC14
Hi,
I'm trying to configure pin PC14 to be used as SDA signal as it stated in the datasheets STM32C031C6 and STM32C031G4:


To configure the pin (and the the I2C) I am using:
void SDK_I2C_Init(SDK_I2C_HandleTypeDef *hi2c) {
LL_I2C_InitTypeDef I2C_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
LL_RCC_SetI2CClockSource(LL_RCC_I2C1_CLKSOURCE_PCLK1);
LL_IOP_GRP1_EnableClock(LL_IOP_GRP1_PERIPH_GPIOB);
LL_IOP_GRP1_EnableClock(LL_IOP_GRP1_PERIPH_GPIOC);
/**I2C1 GPIO Configuration
PB8 ------> I2C1_SCL
PC14 ------> I2C1_SDA
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_8;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_OPENDRAIN;
GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;
GPIO_InitStruct.Alternate = LL_GPIO_AF_6;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_14;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_OPENDRAIN;
GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;
GPIO_InitStruct.Alternate = LL_GPIO_AF_14;
LL_GPIO_Init(GPIOC, &GPIO_InitStruct);
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_I2C1);
I2C_InitStruct.PeripheralMode = LL_I2C_MODE_I2C;
I2C_InitStruct.Timing = I2C_TIMING;
I2C_InitStruct.AnalogFilter = LL_I2C_ANALOGFILTER_ENABLE;
I2C_InitStruct.DigitalFilter = 2;
I2C_InitStruct.OwnAddress1 = 180;
I2C_InitStruct.TypeAcknowledge = LL_I2C_ACK;
I2C_InitStruct.OwnAddrSize = LL_I2C_OWNADDRESS1_7BIT;
LL_I2C_Init(I2C1, &I2C_InitStruct);
LL_I2C_EnableAutoEndMode(I2C1);
LL_I2C_SetOwnAddress2(I2C1, 0, LL_I2C_OWNADDRESS2_NOMASK);
LL_I2C_DisableOwnAddress2(I2C1);
LL_I2C_DisableGeneralCall(I2C1);
LL_I2C_EnableClockStretching(I2C1);
LL_I2C_Disable(I2C1);
LL_I2C_SetTiming(I2C1, I2C_TIMING);
LL_I2C_Enable(I2C1);
}
which is almost the same code that we can find here.
If I configure another pin to work as SDA (PB9 or PB7) the system works perfectly and I can communicate using the I2C protocol.
Is there any configuration that I am missing for that specific pin?